Using Kollmorgen Visualization Builder

To work with Kollmorgen Visualization Builder, do as follows:


  • Be aware that as soon as you change the PLC variables exported for the HMI, the mapping file must be re-imported in Kollmorgen Visualization Builder to have an up-to-date version.

Related Documents

For further information on Kollmorgen Visualization Builder, refer to the following manual:

KVB Guide   Description
Kollmorgen Visualization Builder™ Quick Start Guide Quick Start that covers the most important points to install and use Kollmorgen Visualization Builder, in order to configure HMI Panels and PC operated control applications
Kollmorgen Visualization Builder™ User Manual Contains all the content to help you with Kollmorgen Visualization Builder

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen